Hi, I have the following questions looking forward to your answers :
1) When the radar board is transmitted to the respiratory heart rate GUI on the PC through the serial port, which stage is the data in the following figure? Which step is the data given by the radar board and which step is the data processed by the subsequent software?
2) Step 6 is implemented in which code in which file?
3) Respiratory heart rate demo is calculated by GUI software or hardware output to the computer data bin file there, if it is software calculation please ask his source code where?
4) If I want to use the save data of the GUI interface of the driver vital signs demo to save data, what should I do to extract complex range bin drawings?

Thank you so much.