Other Parts Discussed in Thread: AWR2944, , AWR2243
1. In AWR2944 EVM, which parameters in cfg needs to be changed in order to increase the range profile in 3D up-to 150meters with/without any compromise in the resolution? Please be noted that the example used for testing was awr2944_mmw_demoTDM, and demo visualizer tool. cfg attached.
2. Also, what is the out-of-box demo that needs to be considered to use beyond 100+ meters?
3. Is there any beam steering feature available in AWR2944EVM and if yes where can we find the inbuilt code/demo and how to enable it?
4. Is there any matlab code available with the package of 2944, just like AWR2243 cascade radar?