This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: In DDMA Metric calculation, how to use the SHUFFLE function of HWA to control the position of input points?

Part Number: AWR2944


In DDMA Metric calculation, how to use the SHUFFLE function of HWA to control the position of input points? I didn't see a detailed description of this parameter in the HWA2.0 user manual. Could you give me an example?

In the 2944DDMA demo, how does the shuffler here get in HWA?

"HWA SrcAcnt = 4, BCnt=768, SrcAIdx=2, SrcBIdx=2

DstAnt=1, SHUFFLER =[0, 128, 256, 384, 512, 640],

For each Doppler bins in sub-band,
Cyclic sum the power of itself and 3 aliased points in 4
successful sub-band, overall 6 possibility: Z1-Z6

"