Other Parts Discussed in Thread: AWR2944, IWR1843
Hello,
We have recently ordered the AWR2944EVM development kit and are trying to make first test with mmWave Studio in development mode.
All LEDs are correctly lit up and we managed to collect a first set of measures but trying to collect new measures on another day we get an error as seen on the image below. It happens during the RS232 connection (2nd) step in mmWaveStudio. We didn't change anything on the hardware or software side in between both tests.
Is seems to us the error is linked to the USB connection despite everything being set up correctly. We are using mmWave Studio 3.1.1 with up to date drivers and we can see that the XDS110 is detected by the computer (see second image below). We have tried all common fixes such as trying different cables or computers, trying different baud rates, double checking the DCA switches and the AWR2944 jumpers to enable development mode of the radar chip (SOP2), and also inspected the microUSB connection port under a microscope to make sure there are no visible defects.
After the first successful test (when we managed to collect measures) we have documented the entire setup in a 'user guide' which you can also find attached below.
Please let us know if you have any suggestions to solve this issue. We have also made similar tests with the IWR1843 model and it is working perfectly fine.
Kind regards,
Piotr Banach