I'm working with the MRR lab code and I'm having some trouble visualizing multiple points for the same object
In the code, I see the function cfarPeakGroupingAlongDoppler
being used. My understanding is that this function groups peaks along the Doppler direction, but I don't see any similar function being used to group points in Range direction However, when I visualize the results, I only see one point for each object.
Is the range based peak grouping enabled if yes how to disable it .If not then is there any other way that I can get multiple points in same vicinity for the same object.like making the CFAR window smaller .
Regards