Other Parts Discussed in Thread: MMWCAS-DSP-EVM, MMWCAS-RF-EVM, , AWR1243
my environment:
- MMWCAS-DSP-EVM
- MMWCAS-RF-EVM
- AWR2243*4
- windows 11
- matlab 2023b
- PROCESSOR_SDK_RADAR_03_08_00_00
- the board has contacted PC by micro-USB and Network cable
I have followed https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/882929/awr2243-the-appimage-form-sdk3-7-and-sdk3-8-can-not-running-in-cascade-radar-with-awr2243/3344366#3344366 to change code, and build MLO file and APPImage with `MAKECONFIG=tda2xx_cascade_bios_radar` successfully。 But when I run the usecase a: Cascade Radar (4 AWR1243) Capture + Radar Object Detect (DSP) + NetworkTx (TDA2xx Only) and run the `radar_cascade_demo.m`, there was no cloud points in GUI, only the Range Profile can be displayed correctly, as shown in the figure.
What should I do to get the cloud points output?
There is my output log: