This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: IWR1443BOOST no reply the detect data(send again and again)

Part Number: IWR1443BOOST

 Dear Sir

 

Watashi no shitsumon ni taishi, kaki no kaitō o uketorimashita. Sono Chū de," Do you have your debaisu in functional mode?" To iwa rete imasu. Kore wa IWR 1443 BOOST no naka ni functional mode ga hitsuyō to iu kotodesu ka? Sore wa dōsureba nyūshu dekiru no ka, soretomo jibun de sakusei suru no ka? Sakusei suru baai wa hōhō o go kyōji kudasai. Kore ni kansuru shiryō ga areba sono web saito o oshietekudasai. Watashi no shitsumon no kakushin wa, mmwave demo visualizer o shiyō shinaide, CLI tera term matawa python-tō no puroguramu de tsūshin ga kanō ni naruniha nani ga hitsuyō ka to, sono hōhō o shiritai nodesu. Yoroshiku onegaiitashimasu. Mae no mēru (kaki sanshō)de wa functional mode ni settei sa rete iru ka to itte kaki no saito o shōkai sa reta. Sokode wa IWR 1443 BOOST no functional mode no janpa settei o kakunin sa rete iru dakedesu.
さらに表示
Dear Sir
I received the following answer to my question.
It says, "Do you have your device in functional mode?" I would like to ask the following questions regarding this matter.
1. Does this mean that functional mode is required as firmware in IWR1443BOOST?
2. Are these in mmwave_SDK? If not, how can I get one or create one myself?
    If you want to create one, please tell me how. If there is any material regarding this, please let me know the website.
3. How do I install this on IWR1443BOOST?  
What i want to know is "What is required and how can I enable communication with programs such as CLI Tera Term or Python without using 'mmwave demo visualizer'?"
Thank you for your support. 
H.Imabayashi

This time your reply-------------------------------------------------------------

Pedrhom Nafisi replied to IWR1843BOOST: IWR1443BOOST no reply the detect data(send again).

Hello,

Do you have your device in functional mode?

Last time your reply------------------------------------------------------------

Hello H.Imabayashi,

Can you confirm after switching to using a CLI terminal that you have the sensor set to functional mode?

https://dev.ti.com/tirex/explore/node?a=1AslXXD__1.30.01.03&node=A__ACzleIuZ4g1GuBmtlq-cGg__radar_toolbox__1AslXXD__1.30.01.03&placeholder=true

Best Regards,

Pedrhom

Best Regards,

Pedrhom

Industrial mmWave Radar

Applications Engineer

my perception----

In the previous email (see below), I was asked if it was set to functional mode and was introduced to the following site.

There, the functional mode jumper setting of IWR1443BOOST is only checked.