Other Parts Discussed in Thread: TDC7200
Hi,
I designed a ultrasonic ToF measurement PCBA by using the combination of TDC1000 and TDC7200. 10MHz MCLK, 2.5MHz Piezoelectric ultrasonic transducer were used, and run in ToF_MEAS_MODE 0. When run the accuracy evaluation on the test bench. I found its accuray would be around +/-0.5 ns, that's good for me, but it would drift as time goes by.
For example, the first STOP reached at 143.788269 us in the morning, while it would drift to 143.798355 us in the afternoon. As you see, there is about 10 ns drift, and it would even drift to 20 ns sometieme, that's not good for me. So, would you pls help me debug the issue, thanks very much.