Other Parts Discussed in Thread: TDA2
We are attempting to operate with a combination of MMWCAS-DSP-EVM and MMWCAS-RF-RF.
You can proceed in order by looking at the User's Guide for mmWaveStudio 3.1.1, but there are many difficulties.
I installed it following the steps below.
1. Install mmWaveStudio from the installer package
2. Install 32-bit Matlab Runtime Engine (Version 8.5.1)
3. Install Microsoft Visual C++ 2013 Redistributable package
Installation did not proceed even though the FTDI driver was already installed.
The program was executed according to the procedure below.
1. Power up the EVM.
2. To start GUI(mmWaveStudio).
No error message was output and a GUI window appeared.
However, the device was not recognized, so I checked the COM ports and found that only 2 were recognized, not 4 like in the manual.

The picture above is the device manager shown in the user guide.

This is the COM port recognized by my PC.
I'm blocked from here and can't proceed any further.
I tried uninstalling and reinstalling the driver numerous times.
I need some advice.