Other Parts Discussed in Thread: MMWAVE-STUDIO, IWR6843AOP, AWR1843, DCA1000EVM
Hi,
I'm really new to using radar.
Nevetheless, thanks for the Ti video library and Ti Radar academy, I just understood about radar little bit.
I have an idea with using Azimuth-Doppler Heatmap, so I just want to visualize this to test my idea.
But, I can't find any post about this in E2E Forum, and no related content even on the paper.
So, I wonder,
1. Is there any method to make Azimuth-Doppler Heatmap using ADC data with DCA1000
or build my own application without using DCA1000?
2. If yes, Do I have to fix the range to a certain value when I make an Azimuth Doppler heatmap
like azimuth static heatmap fixed the Doppler index to 0?
3. Can I make AD map in Ubuntu environment? (without using mmWave-Studio)
I'm worried that my question might look silly, but I'd appreciate it if you could understand.
Thanks,
Soobin.