Hello Team,
I am having a requirement to monitor DSS clocks where DSP runs on higher clocks during normal operation and when DSP is idle, the clock is switched to low frequency clock. In order to monitor these DSS varying clocks, how can we use the DSS DCC instances?. Is there any option to complete our clock monitoring during DSP run time(High clocks) and complete this before the DSP switches to idle( lower clocks). As per my understanding, the DCC instances are programmable with corresponding counter values which decrements based on the test/reference clocks. So If the clock value changes while counter decrements, the clock monitoring will go wrong. So is there any approach to handle this situation of clock monitoring with varying clocks.
thanks in advance
Sachin