Hi,
I'm testing an AWRL6432 custom board using the qapi_flash_transfer example of mmwave-L SDK 5.3.0.2.
After firmware writing, It doesn't work properly. So I checked the boot info of the export_bootinfo.h.
There was a bit 5 Metaheader not found error in T_BOOT_OBJECT.(value 32)
We use the W25Q16JWXHJQ flash of the WINBOND in the custom board.
Is the flash OK with AWRL6432?? and how can I fix this problem? It works fine on the AWRL6432BOOST EVK board.
Thanks.