This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC1010: How to directly measure board copper temp with HDC1010

Part Number: HDC1010

We are trying to measure the temperature of a copper area on our board which is electrically isolated from any other circuit.  Should we just run a copper bit under the body of the sensor to get this measurement?

  • Hi Daniel,

    Just so I understand, you are trying to sense temperature of a copper region across a HV isolation barrier? I would recommend looking at our new ISOTMP35, which an analog temp sensor designed to be placed across an isolation barrier to directly contact and measure high voltage isolated copper areas.

    May I ask why you have chosen an HDC1010 for this application? Is humidity involved as well? If you are set on using HDC1010, I would recommend placing the sensor as close to the isolation barrier as possible, or like you said running a copper bit under the sensor up to the edge of the isolation barrier. If there is no high voltage and no actual isolation barrier, you could connect a copper trace between the HDC1010 and the copper area you want to sense.

    A picture would be helpful for me to visualize what you are actually trying to do.

    Thanks

    -Alex Thompson

  • Hi Alex,

    We are pretty married to the HDC1010.  I am trying to measure the temperature of a copper area, really a mounting pad for a mechanical assembly but this pad must be electrically isolated from the PCB.

  • Daniel,

    Understood. So yes you could try to run a copper trace from underneath the HDC1010 to the edge of the keep-out region near the heated pad you want to measure. If using the HDC1010 only for temp sensing, you could try to get the sensor as close as possible to the copper pad without violating whatever clearance is required. Lastly, you can try to thermally isolate the HDC1010 on the PCB (so that its reading from the direction of the pad) by placing slot cuts in your PCB on the sides not facing the pad. Air has a much lower thermal conductivity than PCB material, so by adding air gaps in your PCB around any temp sensor you can force the HDC1010 to sense in one direction. If these recommendations aren't helpful or making sense, I would provide a picture (or drawing) of your setup so I can better assist you.

    Regards

    -Alex

  • Hi Alex.  My picture is pretty basic...want to measure the temperature of this standoff without tying the standoff pad to any circuit on our PCB.

  • Daniel,

    Yes all you can really do is place the HDC1010 as close as possible to the standoff, and use slot cuts around the HDC1010 in other areas so it isn't receiving as much thermal energy from other sources.

    Thanks

    -Alex Thompson