hi,
my customer wants to set output frequency like 60, 62, 64 GHz.
They want to test EIRP.
Can I know how to do that?
BR,
frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
my customer wants to set output frequency like 60, 62, 64 GHz.
They want to test EIRP.
Can I know how to do that?
BR,
frank
Hello,
You would need to set the startt frequency to the intended frequency and enable ContStream transmission. Chirp mode woiuld not give the right values for EIRP characterization. You can then use a power meter with a known gain Antenna at a measured distance (preferably in an Anechoic Chamber). Attenuation in the signal from the measured distance can be calculated.
It is important to make sure that the power meter and Antenna will work at the desired frequency. If the power meter is designed for a lower frequency, use a down coverter to down convert the frequency.
Hope this helps.
E. SHareef
hi E. SHareef,
can i know where i can set Start frequencyand enable ContStream transmission?
BR,
frank
E. Shareef,
No, I don't have DCA1000 and never use mmWave Studio before.
correct me if my understanding is wrong.
DCA1000 is to get RF raw data. Customer should have expertise of Radar RF to analyze the raw data.
So, most customers don't have capability and don't need DCA1000.
For EIRP measurement, customer must use DCA1000 + mmWave studio?
BR,
frank
No, DCA1000 is not necessary for EIRP.
The customer must be aware of APIs they are using to send commands to the device. They can use these APIs to radiate into a power meter. Alternatively, they can also use Studio, which is TIs version of a GUI that can be used to send APIs to the device.
Hope this helps,
E. Shareef