Dear Support Team
We need to create a IMDS entry for following part Numbers and need some confirmation as follows:
AWR2944ABSALTRQ1:
(InnoSenT Part Number) 15.00001146
In the material Mold compound a substance "Metal Hydroxide" is entered as Trade Secret. Unfortunately, we cannot draw any conclusions as to which substance this is exactly.
Another substance "Proprietary Filler" is entered in the Substrate material. Here, too, we cannot identify what exactly it is.
A statement regarding REACh is available in the document, but we also need confirmation regarding GADSL (global automotive declarable substance list) that the two substances do not contain any declarable and/or banned substances.
TCAN1057AVDRBRQ1:
(InnoSenT Part Number) 15.00001103
The substance "Proprietary Materials" is entered in the material bond wire. Here we have the same problem as above.
Can you confirm the GADSL conformity?
There is no IMDS ID for both of those parts yet, so we can´t provide any further information
If you have any questions, don´t hesitate to contact me.