is it possible to use the on-board launchPad compatible 40pin connector to trigger external device?
(for example, IP camera with DIO trigger)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Yes this is possible. GPIO_5 is routed to J8.15.
There is however an analog mux, so you must ensure that S1.6 is in the off position.
Please also refer to the gpio example code at: {MMWAVE_L_SDK_INSTALL}\examples\drivers\gpio
Best Regards,
Josh