hi team
We are designing a development board for AWR2944.
Question 1: The TM4C1294NCPDTT3 in TI's EVM realizes the function of XDS110, and its onboard XDS110 is what we really want. If we also place a TM4C1294NCPDTT3 on our development board, does TI provide the corresponding program to turn the TM4C1294NCPDTT3 into an XDS module?
Question 2: If the answer to question 1 is no. We plan to use the XDS110 Debug Probe product for debugging. As far as I know, the TM4C1294NCPDTT3 MCU is used for two reasons: a. JTAG debugging; b. UART data input/output; Can the XDS110 Debug Probe product achieve these functions?
Question 3: Is the FT4232 necessary in the development board? Can the XDS110 Debug Probe product replace the FT4232 in the EVM? If so, I plan to remove the FT4232 from the development board design.
thanks