This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843: Advisory Number Applicable to Errata

Part Number: IWR1843
Other Parts Discussed in Thread: IWR6843,

Hi team,

 

Are there Advisory Number that are not listed in the Errata of IWR1843 but actually apply?

For example, the following is mentioned in the Errata ANA#19 for IWR6843, which I believe applies to IWR1843 as well.

But, there was no mention of ANA#19 in the IWR1843 Errata.

 

ANA#19

Description: A 47-nF capacitor is needed on the bandgap pin. Not having correct capacitor on this

pin, can cause boot up issues, especially, at negative temperatures. This requirement is

being Included in the errata, as it is a recent change which may not be updated in older

reference designs.

Workaround(s): Use the recommended 47-nF capacitor. For example: part - GRM155R71E473KA88.

 

Please let me know if there is Advisory Number that is not listed in the Errata of IWR1843 but actually apply.

Thanks

 

Best regards,

Masahiro Kobayashi