This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432BOOST: visualizer CFG loading/setting values

Part Number: IWRL6432BOOST


I tried differnt .CFG from the MMWAVE_L_SDK_05_04_00_01 Visualizer, 

 'Configuration Selection' in the 'configuration Dashboard', 

found 'Preset Configuration [Object Tracking]' and the CFG file from SDK example folder  values differnt
C:\ti\MMWAVE_L_SDK_05_04_00_01\examples\mmw_demo\motion_and_presence_detection\profiles\xwrL64xx-evm

where can I find the explanation about those argument values?
where the 'preset configuration' stored?

% ****************************************************************
% Configuration Start
% ****************************************************************
sensorStop 0
channelCfg 7 3 0
chirpComnCfg 16 0 0 128 4 28 0
chirpTimingCfg 6 32 0 40 60.5
frameCfg 2 0 200 64 100 0
antGeometryCfg 0 0 1 1 0 2 0 1 1 2 0 3 2.418 2.418
guiMonitor 2 3 0 0 0 1 0 0 1 1 1
sigProcChainCfg 32 2 3 2 8 8 1 0.3
cfarCfg 2 8 4 3 0 12.0 0 0.5 0 1 1 1
aoaFovCfg -70 70 -40 40
rangeSelCfg 0.1 10.0
clutterRemoval 1
compRangeBiasAndRxChanPhase 0.0 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000
adcDataSource 0 adc_data_0001_CtestAdc6Ant.bin
adcLogging 0
lowPowerCfg 1
factoryCalibCfg 1 0 40 0 0x1ff000
boundaryBox -3.5 3.5 0 9 -0.5 3
sensorPosition 0 0 1.9 0 0
staticBoundaryBox -3 3 0.5 7.5 0 3
gatingParam 3 2 2 2 4
stateParam 3 3 12 50 5 200
allocationParam 6 10 0.1 4 0.5 20
maxAcceleration 0.4 0.4 0.1
trackingCfg 1 2 100 3 61.4 191.8 100
presenceBoundaryBox -3 3 0.5 7.5 0 3
microDopplerCfg 1 0 0.5 0 1 1 12.5 87.5 1
classifierCfg 1 3 4
profileSwitchCfg 0 25 25
baudRate 1250000
sensorStart 0 0 0 0
% ****************************************************************


% ****************************************************************
% Configuration Start
% ****************************************************************
% ***************************************************************
% TrackingClassification_MidBw: Chirp configuration and
% processing chain are designed to detect, localize, track, and
% classify objects in indoor or outdoor environments.
% This config utilizes ~1GHz BW (~20cm range resolution) and
% enables all the available six antennas of the EVM.
% The maximum unambigious range of this config is ~10m.
% In this config, auto mode (major and minor) is enabled to track
% objects with any kind of motion, including fine movements.
% ***************************************************************
sensorStop 0
channelCfg 7 3 0
chirpComnCfg 16 0 0 128 4 28 0
chirpTimingCfg 6 32 0 40 60.5
frameCfg 2 0 200 64 100 0
antGeometryCfg 0 0 1 1 0 2 0 1 1 2 0 3 2.418 2.418
guiMonitor 2 3 0 0 0 1 0 0 1 1 1
sigProcChainCfg 32 2 3 2 8 8 1 0.3
cfarCfg 2 8 4 3 0 12.0 0 0.5 0 1 1 1
aoaFovCfg -70 70 -40 40
rangeSelCfg 0.1 10.0
clutterRemoval 1
compRangeBiasAndRxChanPhase 0.0 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000
adcDataSource 0 adc_data_0001_CtestAdc6Ant.bin
adcLogging 0
lowPowerCfg 1
factoryCalibCfg 1 0 40 0 0x1ff000
boundaryBox -3.5 3.5 0 9 -0.5 3
sensorPosition 0 0 1.9 0 0
staticBoundaryBox -3 3 0.5 7.5 0 3
gatingParam 3 2 2 2 4
stateParam 3 3 12 50 5 200
allocationParam 6 10 0.1 4 0.5 20
maxAcceleration 0.4 0.4 0.1
trackingCfg 1 2 100 3 61.4 191.8 100
presenceBoundaryBox -3 3 0.5 7.5 0 3
microDopplerCfg 1 0 0.5 0 1 1 12.5 87.5 1
classifierCfg 1 3 4
baudRate 1250000
sensorStart 0 0 0 0
% ****************************************************************
% Configuration End
% ****************************************************************

  • Hello, 

    The preset configurations options in the visualizer are actually hardcoded within the visualizer source code, they are not accessible. For an explanation of each of the configuration parameters please check this guide. You can refer to the section titled "Configuration (.cfg) File Format"

    Best Regards, 

    Josh