Hi
Could you help suggest that the product is used in cars.
It needs to be able to monitor humidity and needs to be certified by vehicle regulations.
The accuracy does not need to be too high and requires I2C.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Could you help suggest that the product is used in cars.
It needs to be able to monitor humidity and needs to be certified by vehicle regulations.
The accuracy does not need to be too high and requires I2C.
Gareth,
Yes the HDC3021-Q1 is suitable to work in vehicles, could you please tell me more about your application and what vehicle regulations are required here? We have sold HDC3x to other automotive customers so you should be able to use this device right away. The device has a very good RH accuracy of ±2% from 10% to 70% RH (and ±3% to 90% RH) and uses I2C.
But if i know more about your application, needs, and concerns, I can better support you.
Thanks
-Alex Thompson