Other Parts Discussed in Thread: AWR1843AOP, AWR1843
Hi,
I have same questions about AWR1843BOOST EVM and AWR1843AOP EVM.
Question 1, can the demo that runs on the AWR1843BOOST EVM run on the AWR1843AOP EVM in the Beamforming Mode?
Question 2, the radar can detect the object as far as 150m on the AWR1843BOOST EVM.Now if the same demo runs on the AWR1843AOP EVM , can AWR1843AOP EVM detect the object as far as 150m with the same configuration as AWR1843BOOST EVM? Or is it necessary to modify some configurations to achieve the same performance?
Question 3, if it needs to modify some configuration, which parameters should be changed?
Thanks,
BR,
Rata