Hi,
We utilize the AWR2243 in cascade mode and have observed a tendency for our sample signals to decay towards the end of the chirp, as illustrated in the image below.
The chirp configuration was as follows:
- Center frequency: 78.78 GHz
- Chirp slope: 75.027 MHz/µs
- Total Chirp Cycle time: 27.5 µs
- Modulation bandwidth and ADC sampling: 1.50054 GHz
- Chirp Time (RF On): 24 µs
This issue was consistent across all samples tested with the AWR2243 chip. To investigate the issue further, we conducted a laboratory test where we injected two CW signals and used a horn antenna to receive the input. We then compared the IF received signal amplitude versus the CW signal. (see image below)
The results indicated a significant decrease (about 14dB) in gain versus frequency within our chirp bandwidth. However, in the same bandwidth at a different band, we observed much better gain flatness with only about 1dB decrease. see the below image.
Could you suggest any reasons for the significant RX gain drift observed and propose solutions to address this issue?
Thanks