When I try to use the ENCRYP Model to co-design antenna (ex:Patch antenna), it turns out that there're 15 ports in 1 file (AWRL1432_3RX2TX)
I want to make sure:
- How do you suggest costumer use your ANSYS MODEL to do EM simulation?
- What's the fuction of LBK port in EM simulation? Is that nessesary?
- Coud I remove all of the LBK port to reduce the time cost of simulation? (DIE_LBK_Rx1/2/3,DIE_LBK_Tx1/2)
a. The reason why I ask is that the result on smithchart will be different. (Circuit model)
b, When I use 3D EM model of package(including port) I changed the PCB material and drawed antenna on the PCB, I also compared Die_Rx1/2/3 and Die_Tx1/2 only with original(which has both DIE and DIE_LBK) > Result will also be different