Other Parts Discussed in Thread: ENERGIA
Hi all,
My customer is thinking of using the echo data dump function of PGA460.
But it is not working as expected.
Normally, we operate PGA460 (asynchronous).
Only when using the echo data dump function, he would like to use PGA460 in synchronous mode.
The control procedure is as follows:
(1) On-board memory data storage
1. DATADUMP_EN bit set to 1
2. P1_REC bit set to 0x01 to select a recording period with a time length of 8192 μs
3. Burst/Listen command execution
4. SCLK supply (no output in normal case)
5. Data transmitted from PGA460 is H fixed
I expected to transfer 128 bytes of data, but it is H fixed.
(2) Direct Data Burst with USART Synchronization Mode
1. DP_MUX (other than 0x00)
2. SCLK supply (no output in normal case)
3. Command issue (CMD=7 transducer echo data dump)
4. Data transmitted from PGA
*As for the direct data burst operation, the operation has not been confirmed yet.
The echo data dump function is operational.
If you have any countermeasures or procedures, please let me know.
Best Regards,
Ryusuke