Hi,
There are two GPADC supported on AWRL1432, GPADC1 and GPADC2.
With the gpadc example rlexample_gpadcmeas.c, I can get the mean value of GPADC with z_fecssGpadcRes.c_GpadcMeasVa. But I tested on AWRL1432BOOST and found the value of z_fecssGpadcRes.c_GpadcMeasVa[0] is for GPADC2 and the value of z_fecssGpadcRes.c_GpadcMeasVa[1] is for GPADC1. Is this expected? The number of GPADC confused me.
Thanks,
Chris