Other Parts Discussed in Thread: UNIFLASH,
When I flash my board (2944EVM rev B) with the corner radar prebuilt binary (I tried from radar toolbox 1.2, 1.3, 2.0) I get nothing on UART from the board.
I tried flashin using UniFlash and Using the python script. In both cases I get the message that flashing is complete, after which I tried running (with SOPs set correctly) multiple times. Through the python script it says no data on COM port, I also checked the Termina, nothing.