Hello,
I am investigating the use of the IWR6843 device for surface speed measurement of a relatively smooth surface as well as range measurement. These measurements can be separate. The surface speed relative the the radar is~1m/s.
I have 3 Questions:
- Is there an application example (such as xWRLx432 True Ground Speed User Guide) that demonstrates the achievable sensitivity of surface speed measurement with this device?
- To maximise the doppler measurement sensitivity, would there be advantage in configuring the device to operate in CW mode to measure doppler (assuming range was not needed), and does the demonstration software support this?
- Is there a device that might be better suited (assuming save frequency band and similar gain)
Best regards,
David