This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Japan's Radio Certification

Part Number: IWR6843AOP

Hi TI,

We have received some questions from a Japan company on whether it is possible to obtain Japan's Radio certification using the existing millimeter wave sensor demo kit.

1. What is the center frequency, bandwidth, and transmission power used by the millimeter wave sensor. Frequency: 60-64GHz and Transmission Power: 10dBm.
2. Is there a test mode for testing wireless characteristics?
3. Is it possible to set the transmission state to a continuous transmission state other than the intermittent transmission state?
4. Is it possible to set the reception state to continuous reception?
5. Is the transmission power adjustable by command? Yes, transmission power adjustable using the mmWave SDK, command parameters: txOutPower.
6. Is there a career sense function?
7. Is it possible to control the transmission time? (Settings to maximize transmission time and minimize transmission pause time)

Kindly advise on the questions raised above.
If you have further input on the radio's certification, please feedback accordingly.

Best Regards,
jenn