This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP102: A0/B0 dimension

Part Number: TMP102


Hi,

May I know the below A0 and B0 torlerence?

Thanks!

Jeff

  • Hi Jeff,

    Dimensions outlined in the Tape & Reel Information are for the pocket in the tape and are designed to accommodate the device inside. This dimension will be a bit bigger than the device. A0=1.98-2.0mm and B0=1.78-1.8mm. 

    The actual device package dimensions are A=1.5-1.7mm and B=1.1-1.3mm. A=1.6mm nominal (with 0.1mm tolerance) and B=1.2mm nominal (with 0.1mm tolerance).

    Best,

    Sakeenah