In TMP468 datasheet (SBOS762B –NOVEMBER 2016–REVISED JUNE 2017), Table 8 Config Register Bit Description there seems to be an inconsistency in stated POR value. The Table 8 header states the power on reset value for the 16 bit config register is 0x0F9C. In Table 8 row one: Bit field 15:8, name REN8:REN1, the POR value is listed as 1111 1111 which would imply POR value of 0xFF9C.
Is this a document error and if so which is correct config register POR value: 0x0F9C or 0xFF9C?