This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: Internal crosstalk temperature coefficient and phase temperature coefficient

Part Number: OPT3101


Hi Team:

     After completing SDK INLAB_STEP_1, INLAB_STEP_2 and INLAB_STEP_3, the maximum distance measured was only 9m after increasing the crosstalk temperature coefficient. After increasing the phase temperature coefficient, the distance of the measured target changed, and OPT3101 could not follow the change When the temperature of tMain is high, it is above 53℃, and the measured distance was wrong,How to solve these two  problems?

    These are the parameters that I calculated:

    

   

Thanks!