As shown in the figure, a frame of data is collected, but there is a huge gap between chirp amplitude in the middle and chirp amplitude on both sides. May I ask why
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As shown in the figure, a frame of data is collected, but there is a huge gap between chirp amplitude in the middle and chirp amplitude on both sides. May I ask why
Hi Chen,
Thanks for reaching out to us over E2E.
Let me reassign your to an expert.
Regards,
Anirban
Hi Chen,
Can you please confirm that above data is from the TI CAS RF EVM and CAS DSP EVM? If so the this is a known issue that the first chirp data has to be ignored as is corrupted.
Regards
Abhed
yes,the data is from MMWCAS-RF-EVM and MMWCAS-DSP-EVM.The horizontal axis is the number of chirps, and the vertical axis is the number of samples. However, this issue occurs not only on the first chirp, but also on frames other than the first one
Chen,
the first chirp of every frame has to be discarded. Do you see this in other chirps too?
Regards
Hi Chen, This is a known issue and discarding the first chirp of each frame is the only solution.
Regards
hi Abhed ,You may not understand my question.My problem is that chirp is normal when my configuration is chirpperloop=12,numloop=128. However, when I configure chirpperloop = 32 or numloop=255, the chirp amplitude is different for each frame. My problem is that chirp is normal when my configuration is chirpperloop=12,numloop=128. However, when I configure chirpperloop = 32 or numloop=255, the chirp amplitude is different for each frame.
Hi Chen,
Did you try reducing the number of chirps or loops? Also please confirm when you say chirp amplitude is difference for each frame, then is it just the first chirp or every chirp? If it is first chipr then my previous statement stands ture irrespectively.
I have tried to reduce chirp and loop, chirp is normal only when chirpnum =12,loopnum=128, in other configurations there are a lot of chirp in a frame with different amplitude, this is not the first chirp. I need to transmit a large number of chirp in one frame, numchirp=12,numloop=128 configuration does not meet my needs.