This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Calibration and Object Detection Issue with IWR6843AOP-EVM

Part Number: IWR6843AOPEVM

Hello,

I'm reaching out regarding an issue I've encountered while using the IWR6843AOP-EVM for extracting the compRangeBiasAndRxChanPhase parameters, as outlined in the "Detection Layer Parameter Tuning Guide for the 3D People Tracking Demo – Rev 3.1."

To provide context, I've followed the prescribed steps meticulously. This includes utilizing the demo binary and calibration profile from "mmwave_sdk_03_05_00_04\packages\ti\demo\xwr68xx\mmw" and adhering to the calibration procedure documented in "mmwave_sdk_03_05_00_04/packages/ti/demo/xwr68xx/mmw/docs/doxygen/html/index.html." Additionally, I've placed a metal reflector measuring 12cm by 15cm, positioned at 1m from the sensor during calibration.

Enclosed with this email, you'll find visual representations in the form of Range-Profile and Azimuth-Range-Heatmap graphs. Furthermore, I've included a snippet of the calibration parameters printout for your reference.

compRangeBiasAndRxChanPhase 0.0731140 0.23532 -0.81952 -0.37357 0.75186 0.39874 -0.62717 -0.28342 0.72424 0.23337 -0.95166 -0.44833 0.89386 0.41525 -0.76297 -0.31064 0.84314 0.21487 -0.89243 -0.39841 0.82614 0.39572 -0.70679 -0.29651 0.78278

To refine the configuration, I've averaged parameters over 10 samples and integrated them into the original config file of the People Counting Project located in "mmwave_industrial_toolbox_4_12_0\labs\People_Counting\3D_People_Counting\chirp_configs\ AOP_6m_default.cfg." Additionally, I've adjusted the sensor position within the config file to "sensorPosition 3.0 45 35” to accommodate a 35-degree tilt of the EVM module.

However, despite these measures, I've encountered an unexpected discrepancy in object detection. Specifically, when evaluating the height of a "13cm X 13cm" PC fan positioned vertically on the floor at coordinates X=1m and Y=5.4m, the detected height registers as Z=43cm. This contrasts starkly with the anticipated maximum height of 12cm.

Any insights or guidance you can offer to solve this issue would be appreciated.

Regards,

Kai