Hi Team,
I want to confirm if there is any small package of TMP61 will be pushed such as DYY, DDF, DDC... And could you share the small package information and RTM time if we have. Thanks.
Best Regards,
Ryker
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ryker,
These are all larger packages than what we currently offer.Currently there are no plans to build TMP61 in any of these as I do not believe that these are commonly used for thermistors in the market. Is there customer intested on these for TMP61?
Best regards,
Simon Rojas
Hi Simon,
I want to confirm that if we will push smaller package of TMP61?
Best Regards,
Ryker
Hi Ryker,
Not sure which form factor you are reffering to. As mentioned before, all of these (DYY, DDF, DDC) are larger than what we currently offer. In addition, this is a 2 pin device--the packages mentioned seem to all be for 5 to 6 pin devices.


The only way in which this could be made even smaller would be an 0201 form factor which we do not have any plans to do right now. If you have a specific customer inquiry about this please feel free to reach out over email.
Best regards,
Simon Rojas