Other Parts Discussed in Thread: IWR6843, IWRL6432, SYSCONFIG
According to the MMW Demo documentation the same serial port that we use to send commands to the device is used to transmit the TLV messages:
My EVM board uses ttyACM2 for CLI commands. Is there any existing code or configuration that will let me easily change the output serial port, the one through which TLV messages get transmitted, to ttyACM3? Or do I need to write this configuration myself?
As we all know, the IWR6843 uses two serial ports, one for CLI commands and one for TLV messages. I'd like to have this same separation using the IWRL6432. I'm not entirely sure how to stop the sensor (other than pressing the reset button or power cycling) if I don't....
Thanks