This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: AWR1243BOOST

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: AWR1243, UNIFLASH

We are experimenting with AWR1243 (along with DCA1000). After successfully installing on this window laptop :
mmwave_studio_02_01_01_00
mmwave_dfp_01_02_06_03
xds_drivers
Uniflash

we are still unable to flash the part. Either thru Uniflash or thru the mmdevstudio. We have tried to run the executable in dfp called mmwave-example.exe directly and even that 
fails due to not being able to reset the board. Please see below
-----------------------------------------------------------------------------

C:\ti\mmwave_dfp_01_02_06_03\ti\example\mmwavelink_example>mmwavelink_example.exe
=========== mmWaveLink Example Application ===========
Device map 1 : SOP 4 mode successful

Device map 1 : Device reset successful

rlComIfOpen Callback Called for Device Index [0]
rlDeviceEnable Callback is called by mmWaveLink for Device Index [0]
mmWave Device Power on failed for deviceMap 1 with error -8

=========== mmWaveLink Example Application execution Failed ===========

=========== mmWaveLink Example Application: Exit ===========
----------------------------------------------------------------------------
With Uniflash, when used we get an error "cannot communicate to device error". Even though the serial ports and drivers (4 AR_DEV_pack_EVM012 +2 Emupack XDS110) are seen OK in Device Manager. We can neither erase nor program with this tool as it does not seem to get any response from the AWR1243 card. These cards are brand new. 

_____________________________
In mmdevstudio we tried to connect to USB/FTDI (OK) (step 1) and then fails to load the radarss.bin, or masterss.bin or the meta-file metalmaster.bin as it shows in the status window. 

The AWR boards respond to the reset signal and seem to come out of reset. The DCA1000 unit is starting up well and goes thru its initialization 
goes into a OK mode with Green LED after a full check(LEDs sequencing and flashing at start up). We have directly connected both DCA and AWR to this Laptop (Windows) without the use of a USB hub.

Please assist as we are coming up with a deadline and wanted to get the Radar doing an Azimuth scan of the field on the Laptop.