Hi,
As I asked in other post, if customer wants to receive a range of message ID, range filter and FIFO can be used.
But customer wants to know if similar feature can be implemented on RX buffer or not. That is, can we configure MCAN to receive the message in a range of message ID to one RX buffer?
I checked TRM and found if SFEC=7( Store into Rx Buffer), configuration of SFT[1:0] ignored. Then when SFEC=7, we can only set which(one) message ID to be stored in which(one) RX buffer. Is this understanding correct? If yes, then the answer to above question should be NO, right?
Thanks,
Chris