Hello TI Experts,
I am using AWR1843BOOST and facing some errors at the moment.
I am trying to get as much detected points or point clouds from the radar.
To do so, I disabled grouping by range and doppler, and also trying to lower the cfar range threshold and doppler range threshold.
If I go below certain threshold, both web-based visualizer and python-based visualizer stops.
Some documents mentioned the max number of detected points is 500, but when it stopped it was below the maximum.
I am only trying to parse Detected objects and side info for detected points.
1. What are the limitations of payload size?
2. What are the minimum value I can set as thresholds for both range and doppler?
I would really appreciate if you can guide me with these information.
Sincerely,