This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: For certification

Part Number: IWR6843
Other Parts Discussed in Thread: MMWAVE-SDK

Hello TI,

At first, I am preparing for certification with IWR6843.
I'm using area scanner example.

Below is part of my cfg.

channelCfg 15 7 0
profileCfg 0 60.5 100 25 69 0 0 50 1 256 6000 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
chirpCfg 2 2 0 0 0 0 0 2
multiObjBeamForming -1 0 0.5

Q1. I wonder if the phase shifter will work automatically if I use this configuration.
Q1-1. If the phase shifter operates automatically, please tell me how to disable it.

Q2. Please let me know if there is some way to implement full power CW Tx, which is commonly used for certification.

Q3. Can you explain how to use 3 Txs in the same phase at the same time without using a phase shifter?

Q4. I have seen that using measureRangeBiasAndRxChanPhase command, it is possible to calibrate phase using a corner reflector.
       Please let me know if there is any detailed information on how to calibrate phase and maybe hardware.

Thank you for any help you can offer.

Regards,

--Seokjin