This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: awr2944 secure boot

Part Number: AWR2944EVM
Other Parts Discussed in Thread: AWR2944

Hello

I want to ask a question about secure boot. If otp has been written to the customer keys, awr2944 is converted to type HS-SE. Will the SBL boot the application properly if the HSM Runtime is not runnin?

  • Hi Li,

    No, if HSM runtime is not running, then the secure boot authentication will fail, and the image will not boot. for more information, please refer the TIFS documentation.

    Also, I would suggest you to post the queries in the private forum.

    Regards,

    Shruti