Other Parts Discussed in Thread: IWRL6432
We need to use IWRL6432 for theft protection. Now, we have the IWRL6432BOOST board and we have started working on it. We have some problems to flash binary to board. While we are working on Matlab Radar Toolbox with IWRL6432BOOST eval board, we get an error like the first figure.
Error using untitled (line 5)
Unable to receive data from the TI Radar board. Check if the device is connected, the correct binary is flashed to the device and
the device is in functional mode. To view the steps to flash binary and to set the device in functional mode, run mmWaveRadarSetup
command. If the above actions do not work, try rebooting and resetting the device.
After run the mmWaveRadarSetup command. To flash binary to the board is success. It is not problem in this stage.
However, We get an error " test connection failed." during the data acquisition stage. We are doing the previous steps correctly, we enable functional mode for using SW1 and SW4. What is the reason for this error? Can you help me?