Hi, I am trying out the old build of the occupancy detection visualizer in matlab. i was wondering if its the board connection problem between the device and pc or otherwise?
below i attached the log of the runtime.
Warning: instrfind will be removed in a future release. There is no simple replacement for this.
Opening configuration file C:\Users\msi\Downloads\overhead_occupancy_counter_gui\overhead_occupancy_counter_gui\pc_6843_3d_aop_overhead_3m_radial_low_bandwidth.cfg ...
Warning: The JavaFrame figure property will be removed in a future release. For more information see UI
Alternatives for MATLAB Apps on mathworks.com.
> In overhead_demo_visualizer_occupancy_counter (line 103)
Warning: instrfind will be removed in a future release. There is no simple replacement for this.
Warning: serial will be removed in a future release. Use serialport instead.
If you are using serial with icdevice, continue using serial in this MATLAB release.
Warning: serial will be removed in a future release. Use serialport instead.
If you are using serial with icdevice, continue using serial in this MATLAB release.
Sending configuration from C:\Users\msi\Downloads\overhead_occupancy_counter_gui\overhead_occupancy_counter_gui\pc_6843_3d_aop_overhead_3m_radial_low_bandwidth.cfg file to IWR16xx ...
% TI AOP EVM ID: 1120910143
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
lowPower 0 0
% 040404 = 263172, 050505 = 328965, 060606 = 394758, 080808 = 526344
profileCfg 0 61.0 60.00 11.00 44 328965 0 9.05 1 64 2000.00 2 1 40
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 224 0 110.00 1 0
dynamicRACfarCfg -1 2 39 1 1 4 8 4 4 4.00 6.00 0.50 1 1
staticRACfarCfg -1 1 39 2 2 8 16 4 6 6.00 13.00 0.50 0 0
dynamicRangeAngleCfg -1 7.000 0.0010 2 0
dynamic2DAngleCfg -1 5 1 1 1.00 15.00 2
staticRangeAngleCfg -1 0 1 1
%classifierCfg 1 1 1 500 0.6 1.0 0.95 10
antGeometry0 -1 -1 0 0 -3 -3 -2 -2 -1 -1 0 0
antGeometry1 -1 0 -1 0 -3 -2 -3 -2 -3 -2 -3 -2
antPhaseRot -1 1 -1 1 -1 1 -1 1 -1 1 -1 1
fovCfg -1 62.0 69.0
compRangeBiasAndRxChanPhase 0.0666794 0.83511 -0.47180 -0.85239 0.29214 0.82452 -0.33252 -0.92825 0.36801 0.66608 -0.65576 -0.76456 0.47470 0.69052 -0.53409 -0.78467 0.61990 0.60297 -0.72058 -0.65121 0.63257 0.67444 -0.62360 -0.70523 0.67224
staticBoundaryBox -1.25 1.25 -3 3 -0.5 3
boundaryBox -1.5 1.5 -4 4 -0.5 3
sensorPosition 2.9 0 90
gatingParam 3 2 2 3 4
stateParam 3 3 6 20 3 50
allocationParam 20 20 0.05 7 1.5 20
maxAcceleration 1 1 1
trackingCfg 1 4 800 20 37 33 110 0
presenceBoundaryBox -4 4 -4 4 0.5 2.5
sensorStart
Warning: A timeout occurred before the Terminator was reached.
'serial' unable to read all requested data. For more information on possible reasons, see Serial Read
Warnings.
Warning: The specified amount of data was not returned within the Timeout period.
'serial' unable to read any data. For more information on possible reasons, see Serial Read Warnings.
------------------
Lost sync at frame 1(1), Reason: Header Checksum is wrong, 4880 bytes in Rx buffer
Lost sync at frame 1(2), Reason: Header Checksum is wrong, 4656 bytes in Rx buffer
Lost sync at frame 1(3), Reason: Header Checksum is wrong, 4784 bytes in Rx buffer
Lost sync at frame 1(4), Reason: Header Checksum is wrong, 4560 bytes in Rx buffer
Lost sync at frame 1(5), Reason: Header Checksum is wrong, 4368 bytes in Rx buffer
Lost sync at frame 1(6), Reason: Header Checksum is wrong, 4240 bytes in Rx buffer
Lost sync at frame 1(7), Reason: Header Checksum is wrong, 4080 bytes in Rx buffer
Lost sync at frame 1(8), Reason: Header Checksum is wrong, 3728 bytes in Rx buffer
Lost sync at frame 1(9), Reason: Header Checksum is wrong, 3536 bytes in Rx buffer
Lost sync at frame 1(10), Reason: Header Checksum is wrong, 3536 bytes in Rx buffer
Lost sync at frame 1(11), Reason: Header Checksum is wrong, 3152 bytes in Rx buffer
Lost sync at frame 1(12), Reason: Header Checksum is wrong, 3088 bytes in Rx buffer
Lost sync at frame 1(13), Reason: Header Checksum is wrong, 3152 bytes in Rx buffer
Lost sync at frame 1(14), Reason: Header Checksum is wrong, 2992 bytes in Rx buffer
Lost sync at frame 1(15), Reason: Header Checksum is wrong, 2832 bytes in Rx buffer
Lost sync at frame 1(16), Reason: Header Checksum is wrong, 2544 bytes in Rx buffer
Lost sync at frame 1(17), Reason: Header Checksum is wrong, 2672 bytes in Rx buffer
Lost sync at frame 1(18), Reason: Header Checksum is wrong, 2416 bytes in Rx buffer
Lost sync at frame 1(19), Reason: Header Checksum is wrong, 1904 bytes in Rx buffer
Lost sync at frame 1(20), Reason: Header Checksum is wrong, 2032 bytes in Rx buffer
Lost sync at frame 1(21), Reason: Header Checksum is wrong, 1680 bytes in Rx buffer
Lost sync at frame 1(22), Reason: Header Checksum is wrong, 1520 bytes in Rx buffer
Lost sync at frame 1(23), Reason: Header Checksum is wrong, 1360 bytes in Rx buffer
Lost sync at frame 1(24), Reason: Header Checksum is wrong, 1168 bytes in Rx buffer
Lost sync at frame 1(25), Reason: Header Checksum is wrong, 880 bytes in Rx buffer
Lost sync at frame 1(26), Reason: Header Checksum is wrong, 624 bytes in Rx buffer
Lost sync at frame 1(27), Reason: Header Checksum is wrong, 304 bytes in Rx buffer
Lost sync at frame 1(28), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(29), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(30), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(31), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(32), Reason: Header Checksum is wrong, 304 bytes in Rx buffer
Lost sync at frame 1(33), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(34), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(35), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(36), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(37), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(38), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(39), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(40), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(41), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(42), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(43), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(44), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(45), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(46), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(47), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(48), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(49), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(50), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(51), Reason: Header Checksum is wrong, 108 bytes in Rx buffer
Lost sync at frame 1(52), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(53), Reason: Header Checksum is wrong, 304 bytes in Rx buffer
Lost sync at frame 1(54), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(55), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(56), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(57), Reason: Header Checksum is wrong, 204 bytes in Rx buffer
Lost sync at frame 1(58), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(59), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(60), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(61), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(62), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(63), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(64), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(65), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(66), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(67), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(68), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(69), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(70), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(71), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(72), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(73), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(74), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(75), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(76), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(77), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(78), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(79), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(80), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(81), Reason: Header Checksum is wrong, 304 bytes in Rx buffer
Lost sync at frame 1(82), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(83), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(84), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(85), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(86), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(87), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(88), Reason: Header Checksum is wrong, 304 bytes in Rx buffer
Lost sync at frame 1(89), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(90), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(91), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(92), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(93), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(94), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(95), Reason: Header Checksum is wrong, 464 bytes in Rx buffer
Lost sync at frame 1(96), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(97), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(98), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(99), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(100), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(101), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(102), Reason: Header Checksum is wrong, 368 bytes in Rx buffer
Lost sync at frame 1(103), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(104), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(105), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(106), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(107), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(108), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(109), Reason: Header Checksum is wrong, 368 bytes in Rx buffer
Lost sync at frame 1(110), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(111), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(112), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(113), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(114), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(115), Reason: Header Checksum is wrong, 156 bytes in Rx buffer
Lost sync at frame 1(116), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(117), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(118), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(119), Reason: Header Checksum is wrong, 336 bytes in Rx buffer
Lost sync at frame 1(120), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(121), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(122), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(123), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(124), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(125), Reason: Header Checksum is wrong, 336 bytes in Rx buffer
Lost sync at frame 1(126), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(127), Reason: Header Checksum is wrong, 164 bytes in Rx buffer
Lost sync at frame 1(128), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(129), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(130), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(131), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(132), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(133), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(134), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(135), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(136), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(137), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(138), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(139), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(140), Reason: Header Checksum is wrong, 148 bytes in Rx buffer
Lost sync at frame 1(141), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(142), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(143), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(144), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(145), Reason: Header Checksum is wrong, 272 bytes in Rx buffer
Lost sync at frame 1(146), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(147), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(148), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(149), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(150), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(151), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(152), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(153), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(154), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Lost sync at frame 1(155), Reason: Header Checksum is wrong, 76 bytes in Rx buffer
Lost sync at frame 1(156), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(157), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(158), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(159), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(160), Reason: Header Checksum is wrong, 176 bytes in Rx buffer
Lost sync at frame 1(161), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(162), Reason: Header Checksum is wrong, 304 bytes in Rx buffer
Lost sync at frame 1(163), Reason: Header Checksum is wrong, 208 bytes in Rx buffer
Lost sync at frame 1(164), Reason: Header Checksum is wrong, 240 bytes in Rx buffer
Lost sync at frame 1(165), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(166), Reason: Header Checksum is wrong, 112 bytes in Rx buffer
Lost sync at frame 1(167), Reason: Header Checksum is wrong, 80 bytes in Rx buffer
Lost sync at frame 1(168), Reason: Header Checksum is wrong, 144 bytes in Rx buffer
Warning: The specified amount of data was not returned within the Timeout period.
'serial' unable to read any data. For more information on possible reasons, see Serial Read Warnings.