This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: AWR1843BOOST

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1642, UNIFLASH, AWR1843

Hi,

I'm encountering an issue with the AWR1843BOOST Radar.

When I use the 18xx_mrr code and flash it onto the chip, it begins transmitting data automatically, but the data it sends is consistently corrupted or filled with garbage values.

However, when I utilize the automated_parking_18xx code and configure it through the GUI, it does send data, and the data is accurate.

For my application, I need the system to automatically start and send the correct data, similar to the behavior of the 18xx_mrr code. How can I achieve this?

Another question, why is the MRR code sending wrong data? Is it supposed to be this way?


Regards,
Kartick

  • Hi Kartick,

    Refer to (+) AWR1642BOOST: HARD CODING AND STAND ALONE WORKING OF OUT_OF_BOX_DEMO IN AWR1642BOOST - Sensors forum - Sensors - TI E2E support forums thread and modify cli.c file to bypass the CLI. Update hardCodedConfigCommands with required configuration. Current configuration is for AWR1642 demo.

    why is the MRR code sending wrong data? Is it supposed to be this way?

    Can you be more specific about what the wrong data is? Are you seeing extra objects in visualizer?

    Regards,

    Samhitha

  • Hi Samhitha,

    Thanks a lot for providing the solution. (Let's skip the MRR code part as of now)

    So I followed the following steps for automated_parking_18xx, as mentioned in the article:

    1. Changed the cli.c file (attached in the chat—the one you provided)

    2. Edited setenv.bat file with device name "awr18xx" instead of "iwr16xx"

    3. Executed the setenv.bat and checked (It is working right)

    4. "Make clean" and "Make all" the ti/utils/cli  (new library formed)

    5. Clean and build the dss and mss

    6. Flashed binary file to board using uniflash

    BUT IT IS NOT STARTING AUTOMATICALLY, BUT IS STARTING AFTER INPUT VIA GUI!!

    Do I have to change something in MmwDemo_CLIInit or is there something I am missing?

    MmwDemo_CLIInit code:

    oid MmwDemo_CLIInit (uint8_t taskPriority)
    {
        CLI_Cfg     cliCfg;
        char        demoBanner[256];
        uint32_t    cnt;
    //    static char* dummy[1];
        static char* CLISensorStopArgs[1];
        static char* CLIGuiMonSelArgs[8];
        static char* CLISensorStartArgs[1];
        CLIGuiMonSelArgs[0] = "guiMonitor";
        CLIGuiMonSelArgs[1] = "-1";
        CLIGuiMonSelArgs[2] = "1";
        CLIGuiMonSelArgs[3] = "1";
        CLIGuiMonSelArgs[4] = "0";
        CLIGuiMonSelArgs[5] = "0";
        CLIGuiMonSelArgs[6] = "0";
        CLIGuiMonSelArgs[7] = "1";
        CLISensorStartArgs[0] = "sensorStart";
        CLISensorStopArgs[0] = "sensorStop";
    
        /* Create Demo Banner to be printed out by CLI */
        sprintf(&demoBanner[0], 
                           "******************************************\n" \
                           "xWR18xx MMW Demo %02d.%02d.%02d.%02d\n"  \
                           "******************************************\n", 
                            MMWAVE_SDK_VERSION_MAJOR,
                            MMWAVE_SDK_VERSION_MINOR,
                            MMWAVE_SDK_VERSION_BUGFIX,
                            MMWAVE_SDK_VERSION_BUILD
                );
    
        /* Initialize the CLI configuration: */
        memset ((void *)&cliCfg, 0, sizeof(CLI_Cfg));
    
        /* Populate the CLI configuration: */
        cliCfg.cliPrompt                    = "mmwDemo:/>";
        cliCfg.cliBanner                    = demoBanner;
        cliCfg.cliUartHandle                = gMmwMssMCB.commandUartHandle;
        cliCfg.taskPriority                 = taskPriority;
        cliCfg.socHandle                    = gMmwMssMCB.socHandle;
        cliCfg.mmWaveHandle                 = gMmwMssMCB.ctrlHandle;
        cliCfg.enableMMWaveExtension        = 1U;
        cliCfg.usePolledMode                = true;
        cliCfg.overridePlatform             = true;
    #if defined(USE_2D_AOA_DPU)
        cliCfg.overridePlatformString       = "xWR18xx_AOP";
    #else
        cliCfg.overridePlatformString       = "xWR18xx";
    #endif
            
        cnt=0;
        cliCfg.tableEntry[cnt].cmd            = "sensorStart";
        cliCfg.tableEntry[cnt].helpString     = "[doReconfig(optional, default:enabled)]";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLISensorStart;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "sensorStop";
        cliCfg.tableEntry[cnt].helpString     = "No arguments";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLISensorStop;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "guiMonitor";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <detectedObjects> <logMagRange> <noiseProfile> <rangeAzimuthHeatMap> <rangeDopplerHeatMap> <statsInfo>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIGuiMonSel;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "cfarCfg";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <procDirection> <averageMode> <winLen> <guardLen> <noiseDiv> <cyclicMode> <thresholdScale> <peakGroupingEn>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLICfarCfg;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "multiObjBeamForming";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <enabled> <threshold>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIMultiObjBeamForming;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "calibDcRangeSig";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <enabled> <negativeBinIdx> <positiveBinIdx> <numAvgFrames>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLICalibDcRangeSig;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "clutterRemoval";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <enabled>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIClutterRemoval;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "adcbufCfg";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <adcOutputFmt> <SampleSwap> <ChanInterleave> <ChirpThreshold>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIADCBufCfg;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "compRangeBiasAndRxChanPhase";
        cliCfg.tableEntry[cnt].helpString     = "<rangeBias> <Re00> <Im00> <Re01> <Im01> <Re02> <Im02> <Re03> <Im03> <Re10> <Im10> <Re11> <Im11> <Re12> <Im12> <Re13> <Im13> ";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLICompRangeBiasAndRxChanPhaseCfg;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "measureRangeBiasAndRxChanPhase";
        cliCfg.tableEntry[cnt].helpString     = "<enabled> <targetDistance> <searchWin>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIMeasureRangeBiasAndRxChanPhaseCfg;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "aoaFovCfg";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <minAzimuthDeg> <maxAzimuthDeg> <minElevationDeg> <maxElevationDeg>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIAoAFovCfg;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "cfarFovCfg";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <procDirection> <min (meters or m/s)> <max (meters or m/s)>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLICfarFovCfg;
        cnt++;
        cliCfg.tableEntry[cnt].cmd            = "extendedMaxVelocity";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <enabled>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIExtendedMaxVelocity;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "CQRxSatMonitor";
        cliCfg.tableEntry[cnt].helpString     = "<profile> <satMonSel> <priSliceDuration> <numSlices> <rxChanMask>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIChirpQualityRxSatMonCfg;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "CQSigImgMonitor";
        cliCfg.tableEntry[cnt].helpString     = "<profile> <numSlices> <numSamplePerSlice>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIChirpQualitySigImgMonCfg;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "analogMonitor";
        cliCfg.tableEntry[cnt].helpString     = "<rxSaturation> <sigImgBand>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIAnalogMonitorCfg;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "lvdsStreamCfg";
        cliCfg.tableEntry[cnt].helpString     = "<subFrameIdx> <enableHeader> <dataFmt> <enableSW>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLILvdsStreamCfg;
        cnt++;
        
        cliCfg.tableEntry[cnt].cmd            = "configDataPort";
        cliCfg.tableEntry[cnt].helpString     = "<baudrate> <ackPing>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIConfigDataPort;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "queryDemoStatus";
        cliCfg.tableEntry[cnt].helpString     = "";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLIQueryDemoStatus;
        cnt++;
    
        cliCfg.tableEntry[cnt].cmd            = "calibData";
        cliCfg.tableEntry[cnt].helpString    = "<save enable> <restore enable> <Flash offset>";
        cliCfg.tableEntry[cnt].cmdHandlerFxn  = MmwDemo_CLICalibDataSaveRestore;
        cnt++;
    
        /* Open the CLI: */
        if (CLI_open (&cliCfg) < 0)
        {
            System_printf ("Error: Unable to open the CLI\n");
            return;
        }
        System_printf ("Debug: CLI is operational\n");
    
    
        return;



    The cli.c code that I used (given by you):
    /*
     *   @file  cli.c
     *
     *   @brief
     *      CLI Utility implementation
     *
     *  \par
     *  NOTE:
     *      (C) Copyright 2016 Texas Instruments, Inc.
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *
     *    Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     *    Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the
     *    distribution.
     *
     *    Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /**************************************************************************
     *************************** Include Files ********************************
     **************************************************************************/
    
    /* Standard Include Files. */
    #include <stdint.h>
    #include <stdlib.h>
    #include <stddef.h>
    #include <string.h>
    #include <stdio.h>
    
    /* BIOS/XDC Include Files. */
    #include <xdc/std.h>
    #include <ti/sysbios/knl/Task.h>
    
    /* mmWave SDK Include Files: */
    #include <ti/common/sys_common.h>
    #include <ti/drivers/uart/UART.h>
    #include <ti/utils/cli/cli.h>
    #include <ti/utils/cli/include/cli_internal.h>
    
    /**************************************************************************
     *************************** Hard-coded Configuation **********************
     **************************************************************************/
    #define USE_HARD_CODED_CONFIG
    
    #ifdef USE_HARD_CODED_CONFIG
    
    int32_t hardCodedConfigIndex;
    
    char * hardCodedConfigCommands[] =
    {
    "sensorStop ",
     "flushCfg ",
     "dfeDataOutputMode 1 ",
     "channelCfg 15 3 0 ",
     "adcCfg 2 1 ",
     "adcbufCfg -1 0 1 1 1 ",
     "profileCfg 0 77 7 7 58 0 0  68 1 256 5500 0 0 30 ",
     "chirpCfg 0 0 0 0 0 0 0 1 ",
     "chirpCfg 1 1 0 0 0 0 0 2 ",
     "bpmCfg -1 0 0 1 ",
     "frameCfg 0 1 32 0 100 1 0 ",
     "lowPower 0 1 ",
     "guiMonitor -1 1 1 1 0 0 1 ",
     "cfarCfg -1 0 2 8 4 3 0 15.0 0 ",
     "cfarCfg -1 1 0 8 4 4 1 15.0 1 ",
     "multiObjBeamForming -1 1 0.5 ",
     "calibDcRangeSig -1 0 -5 8 256 ",
     "extendedMaxVelocity -1 0 ",
     "clutterRemoval -1 0 ",
     "compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 ",
     "measureRangeBiasAndRxChanPhase 0 1.5 0.2 ",
     "aoaFovCfg -1 -90 90 -90 90 ",
     "cfarFovCfg -1 0 0.25 9.71 ",
     "cfarFovCfg -1 1 -7.49 7.49 ",
     "CQRxSatMonitor 0 3 4 127 0 ",
     "CQSigImgMonitor 0 63 8 ",
     "analogMonitor 0 0 ",
     "lvdsStreamCfg -1 0 0 0 ",
     "calibData 0 0 0 ",
     "sensorStart ",
     "!!!END_OF_HARD_CODED_COMMANDS"
    };
    
    #endif
    
    /**************************************************************************
     *************************** Global Variables *****************************
     **************************************************************************/
    
    /**
     * @brief   Global variable which tracks the CLI MCB
     */
    CLI_MCB     gCLI;
    
    /**************************************************************************
     **************************** CLI Functions *******************************
     **************************************************************************/
    
    /**
     *  @b Description
     *  @n
     *      The function is the HELP generated by the CLI Module
     *
     *  \ingroup CLI_UTIL_INTERNAL_FUNCTION
     *
     *  @retval
     *      Not Applicable.
     */
    static int32_t CLI_help (int32_t argc, char* argv[])
    {
        uint32_t    index;
    
        /* Display the banner: */
        CLI_write ("Help: This will display the usage of the CLI commands\n");
        CLI_write ("Command: Help Description\n");
    
        /* Cycle through all the registered CLI commands: */
        for (index = 0; index < gCLI.numCLICommands; index++)
        {
            /* Display the help string*/
            CLI_write ("%s: %s\n",
                        gCLI.cfg.tableEntry[index].cmd,
                       (gCLI.cfg.tableEntry[index].helpString == NULL) ?
                        "No help available" :
                        gCLI.cfg.tableEntry[index].helpString);
        }
    
        /* Is the mmWave Extension enabled? */
        if (gCLI.cfg.enableMMWaveExtension == 1U)
        {
            /* YES: Pass the control to the extension help handler. */
            CLI_MMWaveExtensionHelp ();
        }
        return 0;
    }
    
    /**
     *  @b Description
     *  @n
     *      This is the CLI Execution Task
     *
     *  \ingroup CLI_UTIL_INTERNAL_FUNCTION
     *
     *  @retval
     *      Not Applicable.
     */
    static void CLI_task(UArg arg0, UArg arg1)
    {
        uint8_t                 cmdString[256];
        char*                   tokenizedArgs[CLI_MAX_ARGS];
        char*                   ptrCLICommand;
        char                    delimitter[] = " \r\n";
        uint32_t                argIndex;
        CLI_CmdTableEntry*      ptrCLICommandEntry;
        int32_t                 cliStatus;
        uint32_t                index;
    
        /* Do we have a banner to be displayed? */
        if (gCLI.cfg.cliBanner != NULL)
        {
            /* YES: Display the banner */
            CLI_write (gCLI.cfg.cliBanner);
        }
    
    #ifdef USE_HARD_CODED_CONFIG
        hardCodedConfigIndex = 0;
        CLI_write ("Wait some time for system to initialize...\n");
        Task_sleep(100);
        CLI_write ("Performing hard-coded config\n");
    #endif
    
        /* Loop around forever: */
        while (1)
        {
            /* Demo Prompt: */
            CLI_write (gCLI.cfg.cliPrompt);
    
            /* Reset the command string: */
            memset ((void *)&cmdString[0], 0, sizeof(cmdString));
    
    #ifdef USE_HARD_CODED_CONFIG
            /* Run hard-coded commands, one at a time until '!!!END_OF_HARD_CODED_COMMANDS' is reached: */
            if (hardCodedConfigCommands[hardCodedConfigIndex][0] != '!')
            {
                //CLI_write (hardCodedConfigCommands[hardCodedConfigIndex]);
                CLI_write ("Command\n");
                memcpy((void *)&cmdString[0], (void *)hardCodedConfigCommands[hardCodedConfigIndex], strlen(hardCodedConfigCommands[hardCodedConfigIndex]));
                hardCodedConfigIndex++;
            }
            /* Accept commands from UART after all hard-coded commands done: */
            else
            {
                /* Read the command message from the UART: */
                UART_read (gCLI.cfg.cliUartHandle, &cmdString[0], (sizeof(cmdString) - 1));
            }
    
    #else
            /* Read the command message from the UART: */
            UART_read (gCLI.cfg.cliUartHandle, &cmdString[0], (sizeof(cmdString) - 1));
    #endif
    
            /* Reset all the tokenized arguments: */
            memset ((void *)&tokenizedArgs, 0, sizeof(tokenizedArgs));
            argIndex      = 0;
            ptrCLICommand = (char*)&cmdString[0];
    
            /* comment lines found - ignore the whole line*/
            if (cmdString[0]=='%') {
                CLI_write ("Skipped\n");
                continue;
            }
    
            /* Set the CLI status: */
            cliStatus = -1;
    
            /* The command has been entered we now tokenize the command message */
            while (1)
            {
                /* Tokenize the arguments: */
                tokenizedArgs[argIndex] = strtok(ptrCLICommand, delimitter);
                if (tokenizedArgs[argIndex] == NULL)
                    break;
    
                /* Increment the argument index: */
                argIndex++;
                if (argIndex >= CLI_MAX_ARGS)
                    break;
    
                /* Reset the command string */
                ptrCLICommand = NULL;
            }
    
            /* Were we able to tokenize the CLI command? */
            if (argIndex == 0)
                continue;
    
            /* Cycle through all the registered CLI commands: */
            for (index = 0; index < gCLI.numCLICommands; index++)
            {
                ptrCLICommandEntry = &gCLI.cfg.tableEntry[index];
    
                /* Do we have a match? */
                if (strcmp(ptrCLICommandEntry->cmd, tokenizedArgs[0]) == 0)
                {
                    /* YES: Pass this to the CLI registered function */
                    cliStatus = ptrCLICommandEntry->cmdHandlerFxn (argIndex, tokenizedArgs);
                    if (cliStatus == 0)
                    {
                        CLI_write ("Done\n");
                    }
                    else
                    {
                        CLI_write ("Error %d\n", cliStatus);
                    }
                    break;
                }
            }
    
            /* Did we get a matching CLI command? */
            if (index == gCLI.numCLICommands)
            {
                /* NO matching command found. Is the mmWave extension enabled? */
                if (gCLI.cfg.enableMMWaveExtension == 1U)
                {
                    /* Yes: Pass this to the mmWave extension handler */
                    cliStatus = CLI_MMWaveExtensionHandler (argIndex, tokenizedArgs);
                }
    
                /* Was the CLI command found? */
                if (cliStatus == -1)
                {
                    /* No: The command was still not found */
                    CLI_write ("'%s' is not recognized as a CLI command\n", tokenizedArgs[0]);
                }
            }
        }
    }
    
    /**
     *  @b Description
     *  @n
     *      Logging function which can log the messages to the CLI console
     *
     *  @param[in]  format
     *      Format string
     *
     *  \ingroup CLI_UTIL_EXTERNAL_FUNCTION
     *
     *  @retval
     *      Not Applicable.
     */
    void CLI_write (const char* format, ...)
    {
        va_list     arg;
        char        logMessage[256];
        int32_t     sizeMessage;
    
        /* Format the message: */
        va_start (arg, format);
        sizeMessage = vsnprintf (&logMessage[0], sizeof(logMessage), format, arg);
        va_end (arg);
    
        /* If CLI_write is called before CLI init has happened, return */
        if (gCLI.cfg.cliUartHandle == NULL)
        {
            return;        
        }
        
        /* Log the message on the UART CLI console: */
        if (gCLI.cfg.usePolledMode == true)
        {
            /* Polled mode: */
            UART_writePolling (gCLI.cfg.cliUartHandle, (uint8_t*)&logMessage[0], sizeMessage);
        }
        else
        {
            /* Blocking Mode: */
            UART_write (gCLI.cfg.cliUartHandle, (uint8_t*)&logMessage[0], sizeMessage);
        }
    }
    
    /**
     *  @b Description
     *  @n
     *      This is the function which is used to initialize and setup the CLI
     *
     *  @param[in]  ptrCLICfg
     *      Pointer to the CLI configuration
     *
     *  \ingroup CLI_UTIL_EXTERNAL_FUNCTION
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   <0
     */
    int32_t CLI_open (CLI_Cfg* ptrCLICfg)
    {
        Task_Params     taskParams;
        uint32_t        index;
    
        /* Sanity Check: Validate the arguments */
        if (ptrCLICfg == NULL)
            return -1;
    
        /* Initialize the CLI MCB: */
        memset ((void*)&gCLI, 0, sizeof(CLI_MCB));
    
        /* Copy over the configuration: */
        memcpy ((void *)&gCLI.cfg, (void *)ptrCLICfg, sizeof(CLI_Cfg));
    
        /* Cycle through and determine the number of supported CLI commands: */
        for (index = 0; index < CLI_MAX_CMD; index++)
        {
            /* Do we have a valid entry? */
            if (gCLI.cfg.tableEntry[index].cmd == NULL)
            {
                /* NO: This is the last entry */
                break;
            }
            else
            {
                /* YES: Increment the number of CLI commands */
                gCLI.numCLICommands = gCLI.numCLICommands + 1;
            }
        }
    
        /* Is the mmWave Extension enabled? */
        if (gCLI.cfg.enableMMWaveExtension == 1U)
        {
            /* YES: Initialize the CLI Extension: */
            if (CLI_MMWaveExtensionInit (ptrCLICfg) < 0)
                return -1;
        }
    
        /* Do we have a CLI Prompt specified?  */
        if (gCLI.cfg.cliPrompt == NULL)
            gCLI.cfg.cliPrompt = "CLI:/>";
    
        /* The CLI provides a help command by default:
         * - Since we are adding this at the end of the table; a user of this module can also
         *   override this to provide its own implementation. */
        gCLI.cfg.tableEntry[gCLI.numCLICommands].cmd           = "help";
        gCLI.cfg.tableEntry[gCLI.numCLICommands].helpString    = NULL;
        gCLI.cfg.tableEntry[gCLI.numCLICommands].cmdHandlerFxn = CLI_help;
    
        /* Increment the number of CLI commands: */
        gCLI.numCLICommands++;
    
        /* Initialize the task parameters and launch the CLI Task: */
        Task_Params_init(&taskParams);
        taskParams.priority  = gCLI.cfg.taskPriority;
        taskParams.stackSize = 4*1024;
        gCLI.cliTaskHandle = Task_create(CLI_task, &taskParams, NULL);
        return 0;
    }
    
    /**
     *  @b Description
     *  @n
     *      This is the function which is used to close the CLI module
     *
     *  \ingroup CLI_UTIL_EXTERNAL_FUNCTION
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   <0
     */
    int32_t CLI_close (void)
    {
        /* Shutdown the CLI Task */
        Task_delete(&gCLI.cliTaskHandle);
    
        /* Cleanup the memory */
        memset ((void*)&gCLI, 0, sizeof(CLI_MCB));
        return 0;
    }


  • Hi Kartick,

    Update hardCodedConfigCommands with required configuration. Current configuration is for AWR1642 demo.

    Update hardCodedConfigCommands in cli.c with AWR1843 configuration.

    Also check the version of SDK where you updated cli.c file and the version that you are using to build Automated parking demo. If you still see an issue, then delete the project in CCS and import it again.

    Regards,

    Samhitha

  • Thanks a lot Samhitha.

    IT IS WORKING PERFECTLY NOW!!