Hello, I have some questions about the topic: range bin.
I use the vital sign monitoring on the IWR6843AOPEVM and would like to calculate the distance to an object.I only get the range bin from the radar module, so I wanted to calculate the range resolution and estimate the distance.
The calculation is explained in the following article:
I use the following vital_signs_AOP_2m.cfg. file:
According to mmWave Sensing Estimator I get a range resolution of 8.4cm. I wanted to recalculate this using bandwidth, number of samples per chirp and number of range FFT bins.
Question 1:
Using the mmWave Sensing Estimator I have given a Valid Sweep Bandwidth of 1.78025 GHz. However, I actually use a bandwidth of 2 GHz. Which bandwidth is correct now?
Question 2:
What is the Number of Range FFT bins? Where can I get the value?
I would be very grateful for any feedback!
Best regards,
Patrick