This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Extracting Data from mmWave Front-End ADC Without DPU Integration

Part Number: AWR1843BOOST

hello. In the meantime, I developed signal processing by reshaping the 4-channel data from the dumped data using rawdatareader.m using the mmwaveStudio program, and proceeded with the processing. But to select what I will try, I will try to process it with uart and I will reverse the xyz value to find the min position to get it from the demo example already. I want to apply what I create to the data I want.

If you use ccs to confirm that there is a development mode that uses dpu, is it possible to input only the adc data of the mmWaveFrntEnd stage as jtag as shown in the picture without using dpu? Please let me know in detail how it is possible.

What I understood was to flash the radarss firmware to obtain raw data and flash ccsdebug to obtain location data information of signal-processed detected objects. Is this correct?