Part Number: IWRL6432BOOST
Hi All,
Im succesfully doing the demos on the BOOST using the Visualiser in the SDK.
In the Docs section there is a "tuning" document which says you can tune by modifying the cfg in the demos folder.
Some example tuning parameters im interested in (and I'll explain why at the bottom):
Cluster Cfg, Gating parameters.
I looked in multiple files, i couldn't find any simple .cfg file anywhere, and none had those parameters. I've spent along time looking online but Im a bit confused.
I've got the mmwave studio - tried to open but couldnt find any script files, even in the radar toolbox which has a bunch of demos. Not sure how to use them, do I need these?
My use case is I want to "see through" thick grass and detect the distance to bare soil. With the demo this is working already, but I want to make it a bit more robust. And I want to do this on a Rpi. So imagine a stick 2m above some long grass, like 60cm long grass. And the mmWave kit is looking down and detecting distance to the soil.
Could you help me set this up and then get it onto an Rpi5? I think it shouldnt be hard as the demo is working quite well, but some tuning should help!
Kind regards
Fred