This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: meaning of FoVs

Part Number: IWR6843

Hi team,

What do the +/- of these two FoVs mean? Does the total horizontal/vertical detection angle be 130 and 140 degrees?

BR,

Comi

  • Hello Comi,

    Azimuth is horizontal, elevation is vertical. If boresight is directly in front of the sensor at 0 degrees, then for 6843AOP for example you would be able to detect -65 degrees to the left and +65 degrees to the right for a total of 130 in the azimuth. The same for elevation for up and down with the 6843AOP.

    Best regards,

    Pedrhom