Using a STM32H735 devkit with TMP114 sensor connected to the devkit. Scanning for slaves on the i2c bus only detect the onboard audio chip and no TMP114 devices. The sensor have been used in another project with another platform and work fine. But I cannot seams to get any response at all. I use standard mode 100kHz with pullup and no pullup. I can see that I have both data and clock on the bus. Is this device using any specific timing or operation that differs from normal operation?