Few questions:
1. SPI comms:
The data sheet says
1. When comparing the VIH and VIL parameters we see that "MOSI and MISO" are used in both. Can someone please confirm this is a matter of perspective? As in the PGA970 could be operated as a master or a slave - I know later on in the datasheet pg 41 states that the PGA970 can only operate as a slave... so what gives?
2. Why does the VOH and VOL not call out "MOSI or MISO" ?
Waveform Excitation Voltage:
My 4-wire LVDT has a sensitivity of 0.044V/mm/Vex when the excitation voltage is 2.3 Vrms at 5 kHz. I cannot tell through the data sheet if the PGA970 waveform generator is capable of this?