This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: How cloud i process IWR6843ODS raw data captured by DCA1000 to point cloud?

Part Number: IWR6843ISK-ODS


After performing conpon beamforming on adc data, I got the heatmap of range-azimuth and range-elevation. How can I further generate point clouds?  Because the two matrices do not correspond one-to-one in range.

  • Hello,

    Unfortunately we are unavailable to provide high level processing source code for point cloud generation from raw data publicly. We do provide demos that provide you a configurable point cloud which allows additional processing on top of it. I will tell you that we use CFAR, and that you can google and find the procedure of going from raw data, doing the FFTs you need to, and generate a point cloud based on it.

    Best Regards,

    Pedrhom